Everything

-debug


< Optimizing Linkage Editor (rlink) Options / Output Options >

[Format]

-debug

 

-

[Default]

When this option is omitted, debugging information is output to the output file.

[Description]

-

When debug is specified, debugging information is output to the output file.

-

If debug is specified and if two or more files are specified to be output with output, they are interpreted as sdebug and debugging information is output to <first output file name>.dbg.

[Remarks]

-

When form={object | library | hexadecimal | stype | binary}, strip or extract is specified, this option is unavailable.