Everything

-record


< Optimizing Linkage Editor (rlink) Options / Output Options >

[Format]

-record = { H16 | H20 | H32 | S1 | S2 | S3 }

 

-

[Default]

When this option is omitted, various data records are output according to each address.

[Description]

-

Outputs data with the specified data record regardless of the address range.

-

If there is an address that is larger than the specified data record, the appropriate data record is selected for the address.

[Remarks]

-

This option is available only when form=hexadecimal or stype is specified.