Converts a number-representing string to a double type floating-point number.
double strtod (const char *nptr, char **endptr);
nptr Pointer to a number-representing string to be converted
endptr Pointer to the storage area containing a pointer to the first character that does not represent a floating-point number
Normal: If the string pointed by nptr begins with a character that does not represent a floating-point number: 0
If the string pointed by nptr begins with a character that represents a floating-point number: Converted data as a double type floating-point number
Abnormal: If the converted data overflows: HUGE_VAL with the same sign as that of the string before conversion
If the converted data underflows: 0
The strtod function converts data, from the first digit or the decimal point up to the character immediately before the character that does not represent a floating-point number, into a double type floating-point number. However, if neither an exponent nor a decimal point is found in the data to be converted, the compiler assumes that the decimal point comes next to the last digit in the string. In the area pointed by endptr, the function sets up a pointer to the first character that does not represent a floating-point number. If some characters that do not represent a floating-point number come before digits, the value of nptr is set. If endptr is NULL, nothing is set in this area.