Calculates the absolute value of an int type integer.
[Format]
#include <stdlib.h>
long abs (long i);
[Parameters]
i Integer to calculate the absolute value
[Return values]
Absolute value of i
[Remarks]
If the resultant absolute value cannot be expressed as an int type integer, correct operation is not guaranteed.