Gets the current rounding direction.
Abnormal: Negative value when there is no rounding direction macro value or the rounding direction cannot be determined
Do not use this function when compiler option nofpu is selected. If used, the function returns a nonzero value, which indicates an abnormality.