Gets the floating-point environment.
[Format]
#include <fenv.h>
long fegetenv( fenv_t *f);
[Parameters]
f Pointer to area to store the floating-point environment
[Return values]
Normal: 0
Abnormal: Nonzero
[Remarks]
Do not use this function when compiler option nofpu is selected. If used, the function returns a nonzero value, which indicates an abnormality.