Outputs a wide string to a stream input/output file.
[Format]
#include <stdio.h>
#include <wchar.h>
long fputws(const wchar_t *restrict s, FILE *restrict fp);
[Parameters]
s Pointer to wide string to be output
fp File pointer
[Return values]
Normal: 0
Abnormal: EOF
[Remarks]
The fputws function is the wide-character version of the fputs function.