Compares two strings specified up to a specified length.
long wcsncmp(const wchar_t *s1, const wchar_t *s2, size_t n);
s1 Pointer to the reference string to be compared
s2 Pointer to the string to compare to the reference
n Maximum number of characters to compare
If string pointed by s1 > string pointed by s2: Positive value
If string pointed by s1 == string pointed by s2: 0
If string pointed by s1 < string pointed by s2: Negative value
The wcsncmp function is the wide-character version of the strncmp function.