Everything
10.2 MESSAGE FORMATS

(1)

When the file name and line number are included

file-name (line-number) : message-type component-number message-number : message

(2)

When the file name and line number aren't included

message-type component-number message-number : message

Remark

Following contents are output as the continued character string.

MESSAGE TYPES : 1 alphabetic character
COMPONENT NUMBERS : 05
MESSAGE NUMBERS : 5 digits