Table 10.1
Message Type (CC-RX (V2.00.00 or higher))
Message Type
Description
C
Internal error : Processing is aborted.
No output objects are generated.
E
Error : Processingn is aborted if a set number of errors occur.
F
Fatal error : Processing is aaborted.
M
Information : Informational message.
Check the message and continue the process.
W
Warning : Processing continues.
Output objects are generated (They might not be what the user intended).