2.1 Overview
The resource information tool can be used to confirm the RI600PX resource information (e.g. system information and memory area information) that changes dynamically as the program executes.
Remarks 1. When a program using the RI600PX functionality is downloaded, this panel opens automatically.
2. The value will be indeterminate for the RI600PX resource information shown when the RI600PX system initialization is incomplete, because it will not be managed by the RI600PX.
On the Realtime OS Resource Information panel tabs (e.g. [System] tab and [Memory Area] tab), check the current status of the RI600PX resource information.