Realtime OS Resource Information panel
|
This panel displays the RI600PX resource information (e.g. system information and memory area information) of the RI600PX.
Figure A-1. Realtime OS Resource Information Panel
The following items are explained here.
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
This panel has the following tabs:
(2) Information display area
This area displays the RI600PX resource information (e.g. system information and memory area information) of the RI600PX.
Remark A non-existent state of the resource is supported in RI600PX. Therefore,
"--" is displayed by resource information when a resource is non-existent.