Everything

[Interrupt Handler] tab

This tab displays the interrupt handler information (e.g. Exception Code and Start Address) of the RI78V4.
Figure A-19. [Interrupt Handler] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
This area displays the interrupt handler information (e.g. Exception Code and Start Address) of the RI78V4.
This area consists of the following items.
Exception Code
An icon indicating the interrupt handler of the exception code are shown in the following format.
Icon Exception code
Exception code
Start Address
The start address of the interrupt handler is shown.
Attribute
The attributes of the interrupt handler (coding language of interrupt handler and information of allocation for interrupt handler) are shown in the following format.
Coding language Information of allocation
[Coding language of interrupt handler]
TA_HLNG
C language
TA_ASM
Assembly language
[Information of allocation for interrupt handler]
TA_NEAR
Allocates NEAR areas
TA_FAR
Allocates FAR areas

[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Exception Code, Start Address, Attribute
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
Exception Code, Start Address
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Jump to Source (Start Address)
Opens the Editor panel, and displays the source code of the interrupt handler.
Jump to Disassemble (Start Address)
Opens the Disassemble panel, and displays the results of disassembling the interrupt handler.
Reset Display Item
Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).