Everything

[Initialize Routine] tab

This tab displays the initialize routine information (e.g. Start Address and Extended Information) of the RI78V4.
Figure A-20. [Initialize Routine] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
This area displays the initialize routine information (e.g. Start Address and Extended Information) of the RI78V4.
This area consists of the following items.
Start Address
An icon and the start address of the initialize routine are shown in the following format.
Icon Start address
Extended Information
"-" is shown.
Attribute
"-" is shown.

Remark If the initialize routine information (e.g. Start Address and Extended Information) in each cell is double clicked, then Editor panel displays the source file of the initialize routine, and the caret moves to the corresponding location.
[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Start Address, Extended Information, Attribute
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
Start Address, Extended Information
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Jump to Source (Start Address)
Opens the Editor panel, and displays the source code of the initialize routine.
Jump to Disassemble (Start Address)
Opens the Disassemble panel, and displays the results of disassembling the initialize routine.
Reset Display Item
Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).