Everything

[Extended Service Call Routine] tab

This tab displays the extended service call routine information (e.g. Function Code and Start Address) of the RI850V4.
Figure A-26. [Extended Service Call Routine] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
This area displays the extended service call routine information (e.g. Function Code and Start Address) of the RI850V4.
This area consists of the following items.
Function Code
The function code of the extended service call routine is shown.
Start Address
The start address of the extended service call routine is shown.
Attribute
The coding language of the extended service call routine is shown.
TA_HLNG
C language
TA_ASM
Assembly language

Remark Double-clicking an extended service call routine information cell (such as Function Code or Start Address) displays the source file of the extended service call routine in the Editor panel and moves the caret to the relevant location.
[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Function Code, Start Address, Attribute
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
Function Code, Start Address
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Jump to Source (Start Address)
Opens the Editor panel, and displays the source code of the extended service call routine.
Jump to Disassemble (Start Address)
Opens the Disassemble panel, and displays the results of disassembling the extended service call routine.
Reset Display Item
Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).