Everything

[Timer Queue] tab

This tab displays the timer queue information (e.g. Object Type and Number of Objects) of the RI850V4.
Figure A-29. [Timer Queue] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
(a) First layer
This layer displays the timer queue information (e.g. Object Type and Number of Objects) of the RI850V4.
This layer consists of the following items.
Object Type
An icon indicating the current status of the timer queue and the object type are shown in the following format.
Icon Object type
[Icon]
There are queued tasks.
There are no queued tasks.
There are queued cyclic handlers.
There are no queued cyclic handlers.
[Object type]
Task
Task
Cyclic Handler
Cyclic handler
Number of Objects
The total number of queued objects (tasks and cyclic handlers) is shown.

(b) Second layer
<1> Waiting task information
The waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the timer queue.
See the [Task] tab for details about waiting task information.
Figure A-30. [Timer Queue] Tab (Waiting Task Information)
Remarks 1. Double-clicking a waiting-task information cell (e.g., Object Name or ID) displays the source file of the task in the Editor panel and moves the caret to the relevant location.
2. Double-clicking the waiting-task information cell for Current Task Stack SP or Task Stack Area displays the contents of the task stack in the Memory panel and moves the caret to the relevant location.
<2> Cyclic handler information
The cyclic handler information (e.g. Cyclic Handler Name and ID) only appears if there are cyclic handlers queued in the timer queue.
See the [Cyclic Handler] tab for details about cyclic handler information.
Figure A-31. [Timer Queue] Tab (Cyclic Handler Information)
Remark Double-clicking a cyclic handler information cell (such as Cyclic Handler Name or ID) displays the source file of the cyclic handler in the Editor panel and moves the caret to the relevant location.
[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Object Type, Number of Objects
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
Number of Objects
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Reset Display Item
Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).