Everything
2.3.2 [Full-spec emulator]/[IE850A]/[E1]/[E20]/[E2]

Configure the operating environment on the Property panel below when using Full-spec emulator, IE850A, E1, E20, or E2.

Caution

Only LPD communications are supported for communication with the target board.

Figure 2.6

Example of Property Panel

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

[Connect Settings] tab

[Debug Tool Settings] tab

[Download File Settings] tab

[Flash Options Settings] tab

[Hook Transaction Settings] tab