Everything
2.15.2 Measure execution time in a section

In the program execution process, the execution time in a section can be measured by setting Timer Result event.

To use this function, follow the procedure described below.

 

2.15.2.1 Set a Timer Result event

2.15.2.2 Execute the program

2.15.2.3 Edit a Timer Result event [Full-spec emulator][E1][E20]

2.15.2.4 Delete a Timer Result event

Caution 1.

Also see "2.19.7 Notes for setting events" for details on Timer Result events (e.g. limits on the number of enabled events).

Caution 2.

To use this function, [Yes] must be specified with the [Use timer function] property in the [Timer] category on the [Debug Tool Settings] tab of the Property panel.