The core (PE) to be debugged can be selected in either of the following two ways.
Select a desired PE from the drop-down list (shown below) on the statusbar in the Main window.
When the drop-down list used for switching between cores on the status bar is being displayed while the size of this window is maximized, part of the list is hidden behind the task bar and thus cannot be selected. |
Select a desired PE on the Debug Manager panel that are opened by selecting [Debug Manager] from the [View] menu.