A breakpoint is one of the break events that can be set by one-clicking with the mouse.
The program in execution can be stopped at the arbitrary position easily by setting a breakpoint.
This section describes the following operations.
2.11.3.1 Set a breakpoint
2.11.3.2 Edit a breakpoint
2.11.3.3 Delete a breakpoint