Everything
2.3.7 [Simulator]

Configure the operating environment on the Property panel below when using Simulator.

Figure 2.12

Example of Property Panel [Simulator]

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

[Connect Settings] tab

[Debug Tool Settings] tab

[Download File Settings] tab

[Hook Transaction Settings] tab

 

Remark 1.

When the simulator of the selected microcontroller supports peripheral function simulation, it simulates the peripheral functions for the given type of microcontroller.When Simulator to be used corresponds to peripheral function simulations, you can use the Simulator GUI. See "2.19 Use the Simulator GUI [Simulator]" for details on the Simulator GUI. Refer to the release note for details on the peripheral function simulation.

Remark 2.

When the simulator of the selected microcontroller does not support the simulation of peripheral functions, it operates as an instruction simulator.
Refer to the 2.22 RL78 Instruction Simulator [Simulator] for details on the Instruction simulation.

Remark 3.

When the selected microcontroller incorporates a flexible application accelerator (FAA), the RL78 instruction simulator also simulates the FAA. For details on the function of simulating the FAA, refer to the release note for the RL78 simulator which handles simulation of the peripheral functions.