2.13.1
Configure the timer operation
Before the timer function can be used, it is necessary to make settings relating to the operation of a timer.
Note that the method on how to set differs depending on the debug tool used.
2.13.1.1 [IECUBE]
2.13.1.2 [Simulator]