Everything
2.13.3 Measure execution time in a section [IECUBE][Simulator]

In the program execution process, the execution time in a section can be measured by setting Timer Result event. This Timer Result event consists of a timer start event and a timer end event.

To use this function, follow the procedure described below.

 

2.13.3.1 Set a Timer Result event

2.13.3.2 Execute the program

2.13.3.3 Edit a Timer Result event

2.13.3.4 Delete a Timer Result event

 

Caution 1.

[E1][E20][EZ Emulator][COM Port]
Timer Result event is not supported.

Caution 2.

Also see "2.16.7 Notes for setting events" for details on Timer Result events (e.g. limits on the number of enabled events).