You can change the download files and the condition to download.
With CS+, the following file types can be downloaded.
You can change the download files or download conditions in the following Download Files dialog box.
The Download Files dialog box is opened by clicking the [...] button that appears at the right edge in the column of the [Download files] property when you select it in the [Download] category on the [Download File Settings] tab of the Property panel.
This section describes how to configure on the Download Files dialog box above when the following cases.
For details on the contents and function in each area, see the section for the Download Files dialog box.
2.6.2.1 Change download conditions for load module files
2.6.2.2 Add download files (*.hex/*.mot/*.bin)
2.6.2.3 Perform source level debugging with files other than the load module file format