Everything
2.6.2.2 Add download files (*.hex/*.mot/*.bin)

Follow the steps below to add download files other than the load module format (Intel HEX file (*.hex), Motorola S-record file (*.mot) or binary file (*.bin)) in the Download Files dialog box.

(1)

Click the [Add] button

When the [Add] button is clicked, a blank list item "-" is displayed in the last line of the [Download file list] area.

(2)

Property configuration of the download files to add

Configure the download conditions for the download file to add in the [Download file property] area.

Configure each item displayed with the following condition.

When the configuration is completed, the file name specified in this property is displayed in the blank list of the [Download file list] area.

File

Specify the download file (Intel HEX file (*.hex), Motorola S-record file (*.mot) or binary file (*.bin)) to download (up to 259 characters).

Default

Blank

Modifying

Directly enter from the keyboard, or specify with the Select Download File dialog box that is opened by clicking the [...] button.

Available values

See "Table 2.2 Downloadable File Formats".

File type

Specify the type of the file to download.

Select [Hex file] or [Binary data file].

Default

Load module file

Modifying

Select from the drop-down list.

Available values

Either one of the following

-

Load module file

-

Hex file

-

S record file

-

Binary data file

Offset

Specify the offset from the address at which the file's download is to start.

Note that this item appears only when [File type] or [S record file] is set to [Hex file].

Default

0

Modifying

Directly enter from the keyboard.

Available values

0x0 to 0xFFFFF in hexadecimal number

Start address

Specify the address at which to start the file's download.

Note that this item appears only when [File type] is set to [Binary data file].

Default

0

Modifying

Directly enter from the keyboard.

Available values

0x0 to 0xFFFFF in hexadecimal number

Remark

The settings of whether to download the object information or symbol information can be made only when the type of the file to download is load module files.

(3)

Check the order of download

The order of the download is the display order of the files displayed in the [Download file list] area.

If you want to change the order, use the [Up]/[Down] button.

(4)

Click the [OK] button

Enable all the configuration in this dialog box and add a download file (the file name is displayed in the [Download] category on the [Download File Settings] tab of the Property panel).