To delete any event you've set, select the subject event and then click the toolbar button .
When an event is specified by a combination of multiple events, each event in the detailed information can be deleted independently.
However, you cannot delete the unconditional trace event and Run-Break timer event, which are the built-in events of the debug tool.
For the timer start and end events, and trace start and end events, you can also delete an event by selecting [Delete Event(s)] from the context menu displayed by right-clicking the event mark that is displayed on the Editor panel or Disassemble panel. |
For the software/hardware break and the trace event consisting of execution-related events, you can delete an event by clicking their event mark that is displayed on the Editor panel or Disassemble panel. |