By setting timer measurement events (timer start event and timer end event) it is possible to measure a program's execution time in any section in its execution process.
To use this function, follow the procedure described below.
2.14.3.1 Setting the timer start event and timer end event
2.14.3.3 Editing a timer measurement event [E1] [E20]
2.14.3.4 Editing timer start and timer end events
2.14.3.5 Deleting a timer start event or timer end event
Also see "2.17.7 Points to note regarding event setting" for details on timer measurement event settings, including the allowable number of valid events. |
[E1(Serial)/E20(Serial) [RX200 Series]] |
[E1] [E20] |