This section describes how to display and change programs when a load module file with the debug information is downloaded to a debug tool.
Downloaded programs can be displayed in the following panels.
Editor panel |
Disassemble panel |
It is normally necessary to download a load module file with debugging information in order to perform the source level debugging, but it is also possible to do so by downloading a hex format (*.hex), Motorola S format (*.mot), or binary data format (*.bin) file (see "2.5.2.4 Performing source-level debug with hex format, Motorola S format, or binary data format files"). |