Everything
2.3 Split the Panel

The Editor panel can be displayed in split form by using the vertical and horizontal splitter bars. The Editor panel can be split in up to two divisions vertically, and two divisions horizontally.

To remove the split, double-click any part of the splitter bar.

Caution

This function is disabled when the Mixed display mode is selected (setting to the mixed display mode removes the split).

Remark

You can also split the panel by double-clicking any part of the splitter.

Figure 2.3

Splitter Bar

Figure 2.4

Vertical/Horizontal Two-way Split View