You can select multiple lines or a block that consists of multiple lines by any one of the following methods.
Editing of the selected contents can be done by using [Cut], [Copy], [Paste], or [Delete] from the [Edit] menu.
Caution | The information of bookmarks (see "2.8Register Bookmarks") is not included in the selected contents. |
(1) | Multiple lines selection |
- | Drag the left-mouse button |
- | Press the [Right], [Left], [Up] or [Down] key while holding down the [Shift] key |
- | Drag the left-mouse button while holding down the [Alt] key |
- | Press the [Right], [Left], [Up] or [Down] key while holding down the [Alt] + [Shift] key |
Figure 2.6 | Multiple Lines Selection and Block Selection |
Caution | If you select a block and paste it on the last line, a new line will be added below the last line. Note that the block will be pasted from the beginning of the new line regardless of where you have tried to paste it within the last line. |