Everything
 

[Pin Function] tab


This tab displays information on each pin of the microcontroller in the order it was grouped into peripheral functions.

Figure A.9

[Pin Function] Tab

 

The following items are explained here.

[How to open]

-

On the Project Tree panel, double-click [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View].

-

On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View], and then press the [Enter] key.

-

From the [View] menu, select [Code Generator 2] >> [Device List View].

[Description of each area]

(1)

Device list view area

This area displays the “device list view” for entering information on the pins of the microcontroller.

The device list view in this area is organized in the order the pins were grouped into peripheral functions.

The following are the columns comprising the device list view.

Pin name

Displays the pin name of the pin.

Available assignment

Displays the summary of function of the pin.

Pin no.

Displays the pin number of the pin.

Pin direction

Displays the pin direction of the pin.

Pin remarks

Displays the precaution on using the pin.

Comment

(maximum 200 characters)

Displays the comment of the pin

Comments can be arbitrarily set up by 200 characters or less