Everything
A.1 Overview

The Code Generator has the following windows, panels and dialog boxes.

Table A.1

Window/Panel/Dialog Box List

Window/Panel/Dialog Box Name

Function

Main window

This is the first window to open when CS+ is launched. This window is used to operate various components (design tool, build tool, etc.) provided by CS+.

Project Tree panel

This panel displays the components of the project (microcontroller, design tool, build tool, etc.) in a tree structure.

Property panel

This panel allows you to view the information on and change the setting for the node selected in the Project Tree panel.

Device List View panel

This panel allows you to enter information on each pin of the microcontroller.

Device Top View panel

This panel displays the information entered in the Device List View panel.

Output panel

This panel displays operation logs for various components (design tool, build tool, etc.) provided by CS+.

Save As dialog box

This dialog box allows you to name and save a file.