Everything

ClearConsole


This function clears the string displayed on the Python console.

[Specification format]

ClearConsole()

[Argument(s)]

None

[Return value]

If the string was cleared successfully: True

If there was an error when clearing the string: False

[Detailed description]

-

This function clears the string displayed on the Python console.

[Example of use]

>>>ClearConsole()
True
>>>