Everything
B.3.1 CS+ Python function (for basic operation)

Below is a list of CS+ Python functions (for basic operation).

Table B.1

CS+ Python Function (For Basic Operation)

Function Name

Function Description

ClearConsole

This function clears the string displayed on the Python console.

CubeSuiteExit

This function exits from CS+.

Help

This function displays the help for the CS+ Python functions.

Hook

This function registers a hook or callback function.

Save

This function saves all editing files and projects.

Source

This function runs a script file.