Everything

common.ConsoleClear


This property sets or refers to whether to clear the display of the Python console when changing the active project.

[Specification format]

common.ConsoleClear = bool

[Setting(s)]

Setting

Description

bool

Set whether to verify during writes.

True: Verify during writes.

False: Do not verify during writes.

[Reference]

Current set value

[Detailed description]

-

This property sets or refers to whether to clear the display of the Python console when changing the active project.

[Example of use]

>>>print common.ConsoleClear
True
>>>common.ConsoleClear = False