Everything

common.Output


This property refers to the execution result or the contents of an error of the CS+ Python function.

[Specification format]

common.Output

[Setting(s)]

None

[Reference]

Execution result or an error message of the CS+ Python function (strings)

Caution

Error messages can only be referred to when the common.ThrowExcept property is set not to throw an exception (False).

Remark

The reference content is retained until the next CS+ Python function call.

[Detailed description]

-

This property refers to the execution result or the contents of an error.

[Example of use]

>>>debugger.Memory.Read("data")
0x0
>>>print common.Output
0