This function terminates the connected CS+, CS+ will be closed.
[Specification format]
[Argument(s)]
None
[Return value]
None
[Detailed description]
- | If no CS+ instance has been connected before via connect() command, an exception will be thrown. |
[Example of use]
>>> import sys
>>> sys.path.append("C:\Program Files (x86)\Renesas Electronics\CS+\CC\Plugins\PythonConsole\integration_service")
>>> import csplus
>>> csplus.connect()
>>> csplus.terminate()
>>>
|