Everything

csplus.get_expression_info


This function gets size, type and value of an expression.

[Specification format]

csplus.get_expression_info(session_id, expression)

[Argument(s)]

Argument

Description

session_id

This argument is ignored in this version.

expression

The expression to be evaluated

[Return value]

Size, type, value of the expression with format: size;type;value

Each information in the return string is described in below.

Value

Description

size

The size in byte of the target expression

type

The type of the target expression

value

The value of the specified expression

[Detailed description]

-

This function gets size, type and value of an expression.

[Example of use]

>>> csplus.get_expression_info(0, "floatVar")
'4;float;10.1234'