Establish socket communication between Python 3 execution environment and CS+.
[Specification format]
[Argument(s)]
None
[Return value]
None
[Detailed description]
- | If the connection cannot be established, an exception will be thrown. |
- | This function must be called before calling other functions. |
[Example of use]
>>> import sys
>>> sys.path.append("C:\Program Files (x86)\Renesas Electronics\CS+\CC\Plugins\PythonConsole\integration_service")
>>> import csplus
>>> csplus.connect()
>>>
|