Everything

csplus.get_all_breakpoints


This function gets information of all breakpoints.

[Specification format]

csplus.get_all_breakpoints()

[Argument(s)]

None

[Return value]

List: The returned list contains information of a breakpoint in the format.

'index, enabled, type, temporary, location'

Value

Description

index

The index of this breakpoint in the list of all breakpoints.

enabled

Whether this breakpoint is enabled or not

type

The type of this breakpoint. Can be "hardware", "software" or "regular"

temporary

Whether this breakpoint is temporary breakpoint or not

location

Information about the location the breakpoint is set.

Can be a number (e.g. "0xffc00000"), a function (e.g. "main") or a source line (e.g. "ccrx.c:30")

[Detailed description]

-

This function gets information of all breakpoints. Only address breakpoint, function breakpoint and line breakpoint will be included in the returned list.

[Example of use]

>>> csplus.get_all_breakpoints()
['0,true,hardware,false,RL78_F13.c:26', '1,true,hardware,false,RL78_F13.c:30']