Below is a list of the panel related to the Python console.
Table A.1
Panel List
Panel Name
Function Description
Python Console panel
You can use IronPython to operate CS+ and the debug tool by command input. You can also register a script with the project by simply displaying the sample script.