Everything
Everything
top
Project Operation
FUNCTIONS
Change the Window Layout
2.11
Change the Window Layout
This section describes how to change the CS+ window layout.
To the latest version of this page
Differences Information
Previous Topic
Information set for each user of the PC
Next Topic
Automatically hide panels
Table of Contents
Overview
Start CS+
Create a Project
Manipulate a Project
Change the Build Tool Version
Set Build Target Files
Make Settings for Build Operations
Run a Build
Verify the Memory Information at Linking
Save the Project File
Change the Window Layout
Automatically hide panels
Float a window
Dock windows
Display multiple panels
Reset the window layout
Accelerate the Startup Time of CS+
Manipulate CS+ on the Command Line