Obtains the logical AND operation for each bit of the first and second term values.
Performs an AND (logical product) operation between the value of the 1st term of an expression and the value of its 2nd term on a bit-by-bit basis and returns the result.
The result "0xA" is returned. Therefore, (1) in the above expression can also be described as:
mov 0xA, r10.