Obtains the logical OR operation for each bit of the first and second term values.
Performs an OR (Logical sum) operation between the value of the 1st term of an expression and the value of its 2nd term on a bit-by-bit basis and returns the result.
Therefore, (1) in the above expression can also be described as: mov 0xF, r10.