Everything
11.17 Function that is specified by #pragma interrupt and for which save_acc is valid has
formal parameters [C/C++ compiler]

If the save_acc flag is valid (including the case when the -save_acc option is specified) for a function specified by #pragma interrupt, formal parameters passed with generation code R4 might not be obtained normally.

 

Note

It is not recommended to define formal parameters for functions specified by #pragma interrupt.