2.17.2  
Displaying only a specific type of event
 
By clicking one of the following toolbar buttons, it is possible to display only a specific type of event. 
| 
  | 
Displays hardware break-related events. | 
| 
  
[E1] [E20] | 
Displays software break-related events.  | 
| 
  | 
Displays trace-related events.   | 
| 
  | 
Displays timer-related events.   | 
| 
  | 
Displays action events (Printf event, interrupt event [Simulator]).   | 
| 
  | 
Displays built-in events (unconditional trace event or Run-Break timer event). Note |