By clicking one of the following buttons, it is possible to jump to the relevant panel corresponding to the address of a currently selected event.
However, these buttons are disabled when a trace event, timer measurement event, or a built-in event (unconditional trace event or Run-Break timer event) is selected.
|
The Editor panel opens, with the caret on it moved to the source line corresponding to the address at which a selected event is set. |
|
|
The Disassemble panel opens, with the caret on it moved to the disassembled result corresponding to the address at which a selected event is set. |
|
|
The Memory panel opens, with the caret on it moved to the memory value corresponding to the address at which a selected event is set. |