The editor features that CS+ provides are implemented by using the Editor panel.
In the Editor panel, the source file is displayed and can be edited. Furthermore, the source level debugging/instruction level debugging and the display of the code coverage measurement resultNote can be performed in this panel.
The code coverage measurement result is displayed only when the debug tool to be used supports the coverage function. |