This class holds function information (return value of the project.GetFunctionList function).
[Type]
class FunctionInfo:
FunctionName = None
FileName = None
ReturnType = None
StartAddress = None
EndAddress = None
|
[Variable]
|
|
|
|
FunctionName
|
This holds the function name.
|
|
FileName
|
This holds the full path of the file that the function is defined.
|
|
ReturnType
|
This holds the type of the return value.
|
|
StartAddress
|
This holds the start address of the function.
|
|
EndAddress
|
This holds the end address of the function.
|
[Detailed description]
[Example of use]
>>>info = project.GetFunctionList()
func1 int 0x00200 0x00224 C:\project\src\test1.c
func2 int 0x00225 0x002ff C:\project\src\test2.c
>>>print info[0].FunctionName
func1
>>>print info[1].FileName
C:\project\src\test2.c
>>>print info[0].StartAddress
512
>>>
|