This class creates conditions for pseudo-timer (parameter of debugger.PseudoTimer.Set function). [RL78 instruction simulator]
[Type]
class PseudoTimerCondition:
VectorAddr = None
Priority = 3
IntervalTime = 1
IntervalTimeUnit = IntervalTimeUnit.Ms
Periodic = False
|
[Variable]
|
|
|
|
VectorAddr
|
Specify the vector address (numerical value: 0, 0x4 to 0x7c, string: the name of a maskable interrupt or “Reset”) of the interrupt which is to be generated when the interval time of the pseudo-timer matches the condition.
Must be specified.
|
|
Priority
|
Specify the interrupt priority (numerical value: 0 to 3).
|
|
IntervalTime
|
Specify the interval time for the pseudo-timer (numerical value: 0x1 to 0xFFFFFFFF).
|
|
IntervalTimeUnit
|
Specify the unit of the interval time.
The following lists the specifiable units.
|
|
|
|
|
IntervalTimeUnit.Min
|
Minutes
|
|
IntervalTimeUnit.S
|
Seconds
|
|
IntervalTimeUnit.Ms
|
Milliseconds
|
|
IntervalTimeUnit.Us
|
Microseconds
|
|
IntervalTimeUnit.Ns
|
Nanoseconds
|
|
IntervalTimeUnit.Clock
|
CPU clock cycles
|
|
Periodic
|
Specify whether an interrupt is to be generated each time the specified time elapses.
True: An interrupt is generated each time the specified interval elapses.
False: An interrupt is only generated once.
|
[Detailed description]
- | "PseudoTimerCondition" is in class format, and the condition of a pseudo timer is set in the variable.
In order to create a condition of a pseudo timer, create an instance, and set conditions for that instance. |